This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Determining when to use SerDes

In reading the LVDS User's Manual it seems ideal to interface an FPGA with a SerDes and transmit data serially.  What is the main driver in deciding to use this approach as opposed to transmitting let's say 10 individual status bits over 10 LVDS pairs, at DC to very low speeds?  It seems the only advantage is cable weight, being that I would need to transmit over 5-10 meters.