Other Parts Discussed in Thread: SN65LVDS109, SN65LVDS104, DS25CP104A
Hi,
I've two short questions.
1. The DS90UB925q is backward compatible with FPD-Link II.
So my question is, is it backward compatible on to ..UR916Q? It is a little bit confusing, because in the datasheet of the UB925Q it isn't mentioned, while in the datasheet of the ..UH925Q it is mentioned.
2. I want to split my LVDS signals (FPD-Link III and/or FPD Link II) in 4 identical signals by using the SN65LVDS109.
Do i have to mind something when i switch the LVDS input of the LVDS109 from FPD-Link II to III?
Best regards
Philipp