Other Parts Discussed in Thread: TXB0108
I am using TXB0108 in my design.Eight LVTTL signals are Transformed by a TXB0108 from 3.3V to 5v frist,then carried by 8 cables(the other end of cables is Suspended).The issue is that the signals are ok when the length of cables is 0.5m,but he signals are bad when the length of cables over 1m.TXB0108 has very ow dc drive strength,is it the reasen?Or the load driving is over 70pF max?Or other reasens esle?