Other Parts Discussed in Thread: LMH0050, LMH0340
The datsheet for LMH0050 states:
The LMH0340/0040/0070/0050 SDI Serializers are part of
National’s family of FPGA-Attach SER/DES products supporting
5-bit LVDS interfaces with FPGAs. An FPGA Host will
format data with supplied IP such that the output of the
LMH0340 is compliant with the requirements of DVB-ASI,
SMPTE 259M-C, SMPTE 292M and SMPTE 424M standards.
See Table 1 for details on which Standards are supported
per device
Where do i find the IP?
Thanks.