Hi,
I'm helping a customer who as the following problem:
I am using the TLK110 Ethernet PHY with a single 3.3V supply. The 1.5V is generated by the TLK110. When I power-up my board with a bench power-supply, the TLK110 freezes. There is no data coming out of the MDIO pin so I cannot even read the PHY Idenfifier Registers. On power-up I hold the RESETN pin of the PHY low until the processor completes initialization (a few seconds). Toggling the RESETN line does not correct the situation. I have noticed that this happens only when the 3.3V rises slowly (50 ms). If I use a different power supply so that Vcc risese more quickly (1 ms) it does not happen. The rise time of the 3.3V should not make a difference since I hold the TLK110 in Reset until the voltage is stable at 3.3V. I have also noticed the when the TLK110 freezes, I can make it functional again by toggling manually the JTAG_TRSTN line. All JTAG pins are unconnected in this design (the JTAG input pins have internal pull-ups). Is this a known issue with the TLK110? Is there another workaround? Why does is seem to be stuck in JTAG mode.
Alex