Other Parts Discussed in Thread: DS92LV16, DS15BA101, DS15EA101
Using the DS92LV16 just for serialization only seems very easy to implement and just with few control pins and without REFCLK. But, unlike the deserialization section, there isn't any feedback status pin on the pll for trasmission, so how can I be sure that the serialization run properly? I'll not have any feedback status from the other DS92LV16 in deserialization configuration that will receive the data.
I will use this device with a cable driver DS15BA101 to drive 20m of cat6 cable. The receiver will be another DS92LV16 with ahead a DS15EA101.
Perhaps connect the +/-RI to +/-DO and monitoring the LOCK? But with the deserialization enabled, the power consumption will double and will be need to supply the REFCLK too.
Thank you
Andrea