Hi,
I have a ULN2003LVDR driving a a 5 volt relay with a coil resistance of 130 ohms.
The ULN2003LVDR (driver) input is driven by an MSP 430 running at 3.6 volts.
The relay is attached to one of the outputs and to +5 volts.
The driver energizes the relay fine but when the MSP430 sets the driver input low again to .002 volts, the driver continues to conduct and not release the relay. The output of the driver stays at about 1.5 volts. Disconnect the relay momentarily from the circuit and the driver returns to the non conducting state.
Relays with ~200 ohms of coil resistance work fine and the relay described above will work OK with a 50ohm resister in series.
Thanks,
Steve