Other Parts Discussed in Thread: TCA9509, PCA9515A, TCA9517
Can the TCA9509 be used as an I2C buffer when both busses are powered from the same Vcc supply voltage (e.g. 3.3VDC)?
The datasheet indicates BUS A running at a max. of Vccb - 1.0V ... so I assume some leakage path to Vccb would be established beyond this limit?
What are the cautions in powering both busses from the same Vcc (is there a workaround for this limitation)?
Customer is Tyco Electronics for Cisco design and they need the small size of the TCA9509RVH package (the PCA9515A ... a possible alternative ... is in a 3by3mm pkg which may be too large). Voltage translation not needed ... package size is design priority.
Thanks,
Phil