This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1310A - Application

Other Parts Discussed in Thread: TUSB1310A

The complication is that I need a serial clock of no more than 3.4 Gbps and the TUSB1310A, yet it  is set up for 5 Gbps. I wonder if it would be possible to connect a 25 MHz clock to the TUSB1310A and configure it for a 40 MHz clock input. That would result, if it works, in an output clock of 25/40 x 5 Gbps = 3.125 Gbps, perfect for this application. Can you investigate the possibility of doing this?