Other Parts Discussed in Thread: SN65HVD231
1) Is it possible to recommend us any low capacitance cable suited for CAN bus applications?
Our system details are:
- Target bitrate: 250kbps
- Max cable length = 200m
- Max nodes = 16
- Transceiver= TI sn65hvd231
We tested above system using unshielded twisted pair but communication struggles when tested on 100m cable.
2) For TI sn65hvd231, can you help us check if TI provides a table of cable distance v.s. terminating resistor values v.s. number of nodes? but we could not find it from TI website.
3) With the stated setup and target speed above, what is the recommended slope control resistor? Is there any technical guide on this subject besides that already in the datasheet?
4) Any info on max number of nodes that the transceiver can support? How does this impact the bus? Is there any technical guide on this subject besides that already in the datasheet?