Other Parts Discussed in Thread: DS92LX1621
Can this chipset operate as a basic, no-frill serdes WITHOUT a microprocessor and I2C conrtol bus present, using its default register values? What if, instead of a twisted pair connection between SER and DES, we use an optical path with a fiber optic transmiiter connected to the SER and a FO recever feeding the DES? There would then be galvanic isolation between the SER and DES and also the communication between SER and DES would be ONE WAY. Would the chipset still function as a no-frills serdes?