Other Parts Discussed in Thread: XIO1100
Hi,
I am trying to get the XIO1100 Phy to produce RX_DATA using external loopback wiring from the TXn/p port to the RXn/p port while supplying TX_DATA, TX_CLK, REFCLK, etc. The issue that I am having is that I cannot get any data when I use the 125MHz single-ended clock for REFCLK+ as defined in the specification. The 100MHz differential clock works fine, but the 125MHz single-ended clock isn't working. I see no output from RX_CLK or RX_DATA. Unfortunately, my end application requires the use of the 125MHz REFCLK.
I am setting the CLK_SEL pin high during reset and setting the REFCLK- pin to VSS as described in the specification.
Any ideas of what I may be doing wrong?
Regards,
Tom