Other Parts Discussed in Thread: DS92LX2121, DS92LX2122
I am working on a design that is using the Channel link III SERDES chip sets DS92LX2121 Serializer and DS92LX2122 Deserializer. The devices are located in separate boxes connected through a 3m Cat5E shielded cable.
When any of the cables attached to Controller or the cable between the Controller and Display are subjected to any noise, such as RF or EFT pulses, the screen flickers. I believe I have tracked it down to being a common mode violation between the Serializer and Deserializer, but I'm not exactly sure how to verify this.
I can provide more details on the system as needed.
Does anyone have any suggestions on what else might cause the screen flicker or possibly have had the same issue?
Here is a block diagram of the system.