Other Parts Discussed in Thread: DS90CR288A, DS90CR287
Hello,
I am designing an HD video input interface that will have multiple videos connected to an input bus. The HDMI and component video receivers have tri-state outputs, but the LVDS receiver/deserializer - DS90CR288A - does not. I was looking at buffers such as the 74LVC245A, 74ALVC245, or 74LVC16245A, however I am concerned with these devices being fast enough. The HD signal is YCbCr 4:4:4, with a clock rate of 74.25MHz. This gives a period of 13.5ns, and the above listed buffers have maximum delta(t)/delta(V) of 5 to 10ns and typical propagation delays of ~3ns. Would any of these buffers work for this application, or are there other options?
Thanks in advance,
Aaron