Other Parts Discussed in Thread: TLK1501, CDCVF25081, CDCVF2310, LMK03806, CDCLVD1208, CDCE62002
I am thinking about using the TLK1501 for this project, but I am interested in what my jitter will be among the end points if I am using multiple TLK1501's.
If my basic flow is 8 parallel paths:
0)data source > TLK1501 transmitter > fiber > TLK1501 receivers > clocked element
1)data source > TLK1501 transmitter > fiber > TLK1501 receivers > clocked element
....
7)data source > TLK1501 transmitter > fiber > TLK1501 receivers > clocked element
I will have a RX_CLK[7:0] from each of my TLK1501 receivers. While my Transmit and Receive latency from each data source to each clocked element can be different for each of the 8 different paths, the latency has to be fixed and near constant. Based on the the TLK1501 datasheet:
The transmit latency will be fixed once the link is established
The receive latency will be fixed once the link is established
The thing that I cannot figure out from the datasheet is the jitter on the RX_CLK. Isn't there some jitter on the RX_CLK which would vary the delay on each of the 8 paths?
1)Is there a way to figure out the RX_CLK jitter based on the datasheet and serial jitter #s?
2)Or should I be looking at a different device to transmit all of this data where I need the delay between the 8 pathways to be near constant.
Thank you