Other Parts Discussed in Thread: LMH1981
Hi Team!
A customer had a question regarding the LMH1981.
Some of their questions came from page 10 under Input Settling Time and Coupling Capacitor Selection.
The value of CIN is a tradeoff between start-up time and jitter performance and therefore should be evaluated based on the application requirements. Figure 11 shows a graph of typical input-referred HSync jitter vs. CIN values to use as a guideline. Refer to the Horizontal Sync Output section for more about jitter performance.
Also they had concerns with the following statement from page 14 of the datasheet under AC-Coupled Video Sources, especially the following statement:
The LMH1981’s input clamp circuitry may have difficulty stabilizing the input signal under this type of shifting; consequently, the unstable signal at VIN may cause missing sync output pulses to result, unless a proper value for CIN is chosen.
Their questions are the following:
What if we don’t care about settling time?
Can I use a 4 uF input cap (with the output being 220uf) and achieve good jitter and lock (even it takes a second)?
Thanks,
Ben