Other Parts Discussed in Thread: TPS2041, TUSB2046B
Hi all,
I am making some modifications to my design and would like to pattern it after the bus-powered, ganged example provided in the datasheet. The only difference in my circuit is that I am only using 3 of the 4 downstream ports. However, I would still like to be able to pull the maximum 100mA per port for a total of 400mA to the device. Will using the TPS2041 as recommended in the datasheet allow me to do this, or will the hub detect that only 3 ports are used and request only 300mA?
If the second case is true, is there a way that I can "trick" the system into providing the maximum current to the device? I have additional circuitry (mainly LEDs) on the board that is not related to any of the downstream USB devices (controller, mouse, keyboard) that I need to power as well.
Thanks,
Brandon