Other Parts Discussed in Thread: TUSB9260, TPS2560
Team,
I know I have seen posts on this before but I haven't really been able to get a definitive answer to the questions that I have below.
1- On Page 19 of the TUSB9260 Demo Board Guide, there is a note saying that the Tx differential pair between TUSB9260 and SATA connector were swapped to simplify board layout and the firmware has taken this swap into account. I’m assuming that the firmware the customer gets with this device doesn’t have this Tx swapping. Is that true? If not, is there a way to get a hold of it. Or should the pins be swapped.
2- Also on page 19, why power pins 38, 49, and 63 for the TUSB9260 device are not lumped in with the other Vdd power pins. One is terminated to USB2_1p1V. Is there a reason for treating these Vdd pins differently?
3- I had to deviate a bit from the reference design because the SATA drive
that we will be powering will require more current and is also powered by +3.3V and not 5V which is what the reference design is doing. So I’m using another TI switcher to produce 3.3V. My question is in regards to the usage of TPS2560 which limits the inrush current. The demo guide recommends using the TPS2560 device. Is it still recommended that I use a TPS2560 with the scenario that I described since now we have the SATA drive being powered by 3.3V and with VBUS being 5V there should be no direct path between the two rails?
Help on this would be greatly appreciated, Thank you in advance.