Other Parts Discussed in Thread: DP83620
Hello,
I'm using the DP83620 PHY in RMII Master mode (RX_DV and TXD_3 are strapped high). The input clock is 25MHz. The RMII Master mode is confirmed by the value of the RMII and Bypass Register (RBR) 0x17 which has value 0x4021. The output from RX_CLK and TX_CLK is 50MHz as expected, while the output from CLK_OUT is 25MHz. I was expecting 50MHz too. Has anybody tried this configuration?
Regards,
Matteo