Other Parts Discussed in Thread: SN65MLVD204A, SN65MLVD047
My design uses a SN65MLVD047APW MLVDS Driver & SN65MLVD204A MLVDS Receiver. 8 receivers are attached to one driver. We recently changed the receiver from a SN65MLVDS200A and want to be sure that the '204A (Type 2) is compatible with the '047 driver. Can you please confirm this?
Also,can you clarify the meaing of the data sheet requirement (page 4) for D|Vyz| = -50mV min, 50mV max for the SN65MLVD047. Is this the difference between the logic-high differential voltage and the logic-low differential voltage?
Thanks.
Ralph Vernile