Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0031 I/O port configuration

How are the timings of Horizontal Sync or Vertical Sync when outputed on I/O port? (I guess it is using Table 6 p27/33.)

Does Hsync =1 between EAV and SAV?

The same for Vsync?


Thanks.

  • The H and V bits are output following the successful decoding of the TRS character string.

    The H-bit is 1 to indicate the EAV sequence, and 0 to indicate the SAV sequence.  This bit is 1 between EAV and SAV (during horizontal blanking), and 0 during active video.

    The V-bit is 1 in the vertical blanking interval, and 0 during active video lines.

    Gary Melchior