Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Industrial Remote I/O

I am looking for a suitable technology to serialize and deserialize signals from an FPGA in an industrial environment.  The goal is to combine many outputs from an FPGA onto a single Cat 5/6 cable and then reproduce those signals at the remote location and combine many inputs at the remote location at the FPGA.  

Requirements:

  1. > 4 signals per twisted pair
  2. Individual signals are < 100 kHz but need < 500 ns jitter.
  3. Cat 6 cables STP
  4. Up to 50 m length
Can anyone suggest the best technology?