Other Parts Discussed in Thread: DS15BA101
Please advise me on interface between DS92LV1021 and DS15BA101.
Can the LVDS output of DS92LV1021 be DC coupled to the differential input of DS15BA101?
The DS15BA101 datasheet specifies the input common mode range as bellow
VICM Input Common Mode Voltage N+, IN- Min 0.8; Max VCC – VVID/2
In other portion of the datasheet describes as bellow:
The IN+ and INpins are self-biased at approximately 2.1V with VCC = 3.3V.
If DS15BA101 input is DC coupled to LVDS output?
Mita