Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[TL16C2550] Frequency tolerance of XTAL input

Other Parts Discussed in Thread: TL16C2550

Hello~

Would you please let me know the Frequency tolerance (PPM???) of XTAL input on TL16C2550 ???

I'm unable to find the value in the TL16C2550 datasheet.

Thanks... C.W. :)

  • Hello C.W.,

    Typically the oscillator inputs can tolerate 100 ppm. The most common crystal oscillators used have a load capacitance of 10 - 22 pF and an ESR of between  20 - 120 ohms.

    Most customers use +/-50 ppm without any problems reported.

    Best Regards,

    Joe