Other Parts Discussed in Thread: DP83848K
DP83848K is configured in mode 2. When there is no connection, the LED_LINK will be OFF.
When there is connection, the LED_LINK will be ON and when there is activity, the LED_LINK will BLINK.
The above scenario happened most of the time, which indicate all the operations are OK.
However, sometimes (1 out of 10 times), some of the phyter chip will show wrong LED_LINK indication (error).
When user turns on the board but there is no connection yet, the LED_LINK will be ON all the time.
However, once the user reset the board or change the IP address, the LED_LINK operation will back to normal
Question: should LED_LINK even turn OFF at all as it is not clearly mentioned in the specs? If so, under what conditions does the light stay ON or OFF?