Other Parts Discussed in Thread: DP83640, DP83630, DP83620
1) WHAT IS THE DIFFERENCE BETWEEN THE DP83640 AND THE DP83630? THE MAIN DIFFERENCE I SEE IS THAT THE DP83630
IS IN A LEADLESS PACKAGE AND IT IS QUITE A BIT LOWER IN
COST. ARE THESE THE ONLY DIFFERENCES?
2) WHAT IS THE DIFFERENCE BETWEEN THE DP83630 AND THE DP83620? THE MAIN DIFFERENCE I SEE IS THAT THE DP83620
DOES NOT SUPPORT IEEE 1588 AND IT IS LOWER IN COST.
ARE THESE THE ONLY DIFFERENCES? WE DO NOT USE IEEE
1588 BUT WE DO REQUIRE SYNCHRONOUS ETHERNET
RECEIVE CLOCK RECOVERY IN RMII MODE. ARE THE
SYNCHRONOUS ETHERNET CAPABILITIES OF THESE TWO PARTS
THE SAME?
Jaden