Other Parts Discussed in Thread: P82B96
Hello,
We are trying to access a peripheral SD card that we have to connect to via a 2'-3' cable, and the interface isn't working with SDIO level translators (tried the ISL3034 and MAX13035E). The Ti equivalents look like they are also designed for a short run between a processor and SD card slot.
We found the following part, http://www.ti.com/lit/ds/symlink/p82b96.pdf, and are interested in using this for an MDIO level translator. However, it could be used in other applications as well. Can this part handle frequencies larger than 400kHz if we have a short cable run? Is there another part that would be more suited for this? We are desperately looking for a part to use for an SD card and the MDIO over cable.
Thanks!