Other Parts Discussed in Thread: LMH0030, LMH0046, LMH0002
I have an LMH0046 being driven by a LMH0030 direct coupled with two 75 ohm pullup resistor on the inputs. The output of the LMH0046 is direct coupled to an LMH0002 with a 100 ohm resistor between the inputs. The 27Mhz is supplied by a 20ppm oscillator. The SDHD output is connected to the LMH002. LF1& LF2 have 56nf cap. lock tied to Mute. Other than power and ground, all other connections are open. The measured input (1080i) to the LMH0046 UI is 0.45, and the output is 0.345UI. This is much too high. What is being done wrong?
Bill