Other Parts Discussed in Thread: ONET1151M, ONET8501T, ONET8501V, ONET1101L
Hi there.
I'm exploring the use of the "11.35-Gbps Differential Modulator Driver with Output Waveform Shaping" http://www.ti.com/product/onet1151m
with the "11.3 Gbps Limiting Transimpedance Amplifier With RSSI" http://focus.ti.com/docs/prod/folders/print/onet8501t.html
The idea is to use rotating mirrors to raster scan a scene and use a beam splitter to work out time-of-flight for each point in the scene.
I'm hoping for a 60 scans per second of 1920x1080 distance measurements in the 5mm-5cm distance range, which I plan to convert into a full HD video stream, with the red, green and blue components combined to produce a 24 bit distance matrix for the scene.
By knowing the mirror angles and the pixel location I can work out the time of flight between the mirrors and determine the round trip time for each pixel independent of its location.
Then I'll use the corrected image to generate a 3D representation of the scene as a point cloud and develop some algorithms to reconstruct the original scene.
Is there an application note for the above devices together, such as a schematic or video, with the part numbers of the emitter/detector + associated circuitry - something I can work off.
Can anyone see any glaring problems with this approach?
Regards,
Philip Ashmore