This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2046B and the 5V Ports (D+ and D-)

Other Parts Discussed in Thread: TUSB2046B, SN75240

Hi,

1) I'm trying to use the TUSB2046B USB HUB Controller, but wenn i designed the schematic i saw that the DM and DP Ports, they are directly with the Outputs connected.

but in every USB are D+ and D- = 5V, if the HUB can work only with 3,3V, How can i connect them?

2) an other question what is the maximum allowed Current for the SUSPEND Port, if i make a LED with a Resitor in series for long time test to this Port?