hello,
I am having difficulties with a circuit i am trying to develop.
it is powered externally with 3.3V as VCC.
the Reset time is 0.02s
The clock only works if the reset is set low (as seen in the schematic) rather than high.
Nothing is attached to its downstream ports at the moment.
Also I would like to know if it is possible to combine two of these hubs together to create a 7way port?
Regards