Other Parts Discussed in Thread: DCH010515D, TL431
Hi All,
I recently designed in the new ISO5500's into our latest inverter, with four driving an H bridge, and one for a buck battery charger. They all drive juicy STGW35HF60WD IGBT's that like a +15V for clean turn on, and -15V for a fast solid turn off. I implemented the design to fig 62 of page 27 of the ISO5500 datasheet.
The problem I have is the ISO5500's (all of them) randomly latch up, gets hot, kills itself and then promptly toasts its Isolated power supply through excessive current draw. My conclusion is that I am hitting the ISO5500 with a short burst of power across VEE and VCC2 that exceed the recommended absolute maximum of 35V at turn on.
Like everyone else, we use unregulated +/- power modules (in our case the VDS series by CUI) these $7 modules are supplied by a switch mode. Both the switch mode and the isolated module supplies have a small amount of over shoot. Further more the isolated supplies are unregulated with a +/- 10% spec, so it is very easy to go over the 35V limit during power on. We need to use 15V for IGBT turn on, we need isolated supplies, and we need low cost. Im not using zeners and TVS to "hopefully" catch the overshoot . However even for normal operation, a 2.5V tolerance on each supply is dangerously close to going poof as it is, unless you use regulators, and thats a lot of circuitry for each supply of each channel (10 in my case).
Does TI have a version of this chip that has a more forgiving tolerance for "Positive output supply Voltage, VOUT+ (VE – VEE-P)" specified on page 4 of the ISO5500 datasheet. As +/-15V IGBT gate drive is very popular? But a mere 5V wont do it for common isolated power supplies, including the DCH01 series, which is all over the place - from 15.2 to 16.2 without taking into consideration of overshoot.
Or does TI have a silver bullet - a DCH01 series with +15V and -9V output - that would perfect. But, I dont think they have.
steve