Hi Ti ,
I'm using DS90UB913Q/DS90UB914Q in one of our designs .
I have configured the Ser/Des pair for 10bit video data with upto 100MHz pixel clock .But as I connect the LVDS cable between the Ser\Des pair I'm seeing the 50MHz pixel clock output coming as a default frequency from the De-Serializer even when there is no camera recording .Once the record is initiated there will be change in pixel clock frequency.
Is it the way the De-Serializer is expected to work as I do not find this information in the datasheet .
Thanks for the reply .
Best Regards,
Rajesh N