Other Parts Discussed in Thread: DS100MB203, SN65LVCP114
Hi Team,
I have a question, Does TI SN65LVCP114 support RXAUI interface like DS100MB203?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS100MB203, SN65LVCP114
Hi Team,
I have a question, Does TI SN65LVCP114 support RXAUI interface like DS100MB203?
Max,
SN65LVCP114 is a buffer based design (NO CDR) so it does support RXAUI data rate of 6.25Gbps.
Thanks,
Atul Patel
Max,
SN65LVCP114 is a mux buffer device not a serdes. So when you say does it support RXAUI I assume you mean that does it support RXAUI data rate which is 6.25Gbps. In this case, SN65LVCP114 can support RXAUI data rate. In use case, SN65LVCP114 and accept multiple RXAUI inputs and perform 1:2/2:1 mux functions on these inputs. If the customer has an application use case diagram please provide it for further clarification. Note, SN65LVCP114 cannot produce a RXAUI link (6.25Gbps) from two inputs of 3.125Gbps.
Thanks,
Atul
Hi Terry,
The SN65LVCP114 does support XFI signalling. The max data rate on the LVCP114 is 14.2Gbps and the linear range of the device is up to 1200mV. This meets all of the specs of the XFI signalling requirements.
Regards,
Mike