Other Parts Discussed in Thread: TPIC6C596, ISO7240C
Currently we have the Pull-Up Resistor at Pin-8 (/G) of TPIC6c596, and Pin-8 (/G) is also connected to CPU.
Thus during power-up, Pin-8 (/G) is pulled to Vcc to disable all 8 Outputs.
After CPU initialization, this Pin-8 (/G) is set to GND by CPU control to enable 8 Output signals.
Now we like to add ISO7240C between TPIC6c596 and CPU for isolation.
(However, this will create more timing issue between two isolated power supplies during power up.)
Will this Pull-Up Resistor still work with ISO7240C?
Do we really need this Pull-Up Resistor or not ?
Best Regards,