Other Parts Discussed in Thread: LMH0344, LMH0303, LMH0384
Hi ,
We are using LMH0303 & LMH0344 in the TX and RX paths of SDI respectively.
SDI TX is working without any issues for all modes (SD-SDI , HD-SDI , 3G-SDI & Dual stream SDI ). We have verified this using SDI Monitor.
Although SDI RX is working fine for SD-SDI & HD-SDI , we are facing issues with 3G-SDI RX .
Due to unavailability of SDI sources , we are using output of one board as the input to other board . With this setup resolution of incoming data is varying continuously.
We tried using LMH0384 (footprint compatible with LMH0344) & with this performance is improved , but the input gets corrupted after 15-20 minutes .
We also observe that this corruption is much more when the SDI TX & RX is operated simultaneously.
Is there any specific things in equalizer we can look into ? Should we increase the drive strength from LMH0303 since this is used as a source ?
Thanks & Regards ,
Suresha.N.S.