This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A problem about C6000 Mcbsp



Hi,

       I have a problem about the Mcbsp of C6416. The setting of XCR is Single-phase frame,2 words in phase 1,Transmit word length is 16 bits. But when I use the oscilloscope to test the FSX and CLKX ,I find that there are 34 clocks in one frame.I think it should be 32 clocks. Why ?  Here is the figure.

Green: FSX

Yellow: CLKX

Set the Mcbsp as SPI mode.