Other Parts Discussed in Thread: TUSB9261, TUSB9260
Hello, is there a timing diagram available for the SPI between the TUSB9261 and the flash memory?
Thanks,
Brian.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Brian,
The SPI interface of the TUSB9261 is controlled by the device itself, including the communication with the flash memory and It has been tested with different models of memories. You can see some examples of these tests and its reached frequencies within the TUSB9260 Implementation Guide, secction 10 ( http://www.ti.com/lit/an/slla301c/slla301c.pdf ).
MANUFACTURER PART NUMBER DENSITY(kbit) PAGE SIZE (bytes) MAX CLOCK FREQUENCY READ COMMAND (MHz)
Numonyx/ST M25P05A 512 256 20 / 25
Numonyx/ST M25P10A 1024 256 20 / 25
Atmel AT25FS010 1024 256 50
Pflash Pm25LV512A 512 256 33
Pflash Pm25LV010A 1024 256 33
Regards,
Diego.
Thanks for the quick reply, Diego. So, does that mean there is no timing diagram available? These parts are old and are generally not available or not recommended for new designs. I would like to use something current, but need to verify the design.
Regards,
Brian.
Hello Brian,
In order to provide you a better support, I want to know if you are looking for the maximum time for the turn-on cycle, or the best SPI performance, or another specific detail. May be faster to solve if I know What I have to look for.
Regards,
Diego
Hi Diego,
Primarily clock to output valid delay time for SS and Data (and which clock edge this is referenced to), and setup/hold times for input data to clock (and which clock edge this is referenced to).
Thanks,
Brian.
Hello Brian
The SPI interface can operate over a frequency range of 100 kHz to 50 MHz, however, the bootloader uses a fixed frequency of 18.75 MHz. The flash must use a word size of 8 bits and an address length of 24 bits. The program instruction must allow 256 bytes to be written in one operation. The set up time is 53 ns and the hold time is 40 ns. The entire chip is erased by the bootloader prior to programming.
Regards,
Diego.
Hello Brian,
The SPI clock is configured as follow: Data is output on the rising edge of SPICLK meanwhile Input data is latched on the falling edge, both have a set up time of 53 ns and the hold time of 40 ns. But I am not sure about the question regarding to to he clock to output valid delay time for SS and Data", because USB3 is asynchronous.
Regards,
Diego.