Other Parts Discussed in Thread: DS90LV012A
I am using DS90LV012A in my design to convert a HCSL input to CMOS output. I have the below queries. The datashheet states that it can have a Vcm in the range of 0.05 to 2.35 volt . HCSL is ground referenced with a Vcm of 350mV . This is within the limits as specified in the datasheet and hence no AC coupling is required. Is my assumption correct.
The DS90LV012A datasheet also states that the max differential swing is 350mV while for HCSL it 700mV. Hence i need to attenuate the signal by adding a series resistor. What is the value I should choose