Other Parts Discussed in Thread: PROFIBUS, SN65HVD1176, SN65HVD1786
Hello,
i´m looking for an profibus transceiver p.e. the SN65HVD1176. These devices has an max. rating of -9 to +14V on any bus I/O terminal, so the transceiver is not protected to an shortcircuit to the 24V power supply lines of the device. In some RS-485 transceiver an protection circuit which withstands up to 70V is allready integrated p.e. the SN65HVD1786.
Does someone knows an Profibus Transceiver with integrated protection circuit?
Or
Is there an alternative remark / recommendation how to solved such protection discreet?
Many thanks