Other Parts Discussed in Thread: SN65LV1224B, SN65LV1023A
Dear All
I am facing some problems with my camera bus.
My camera bus is an 8 bits pixel data with 2 synchronizations lines (horizontal and vertical clock), in other worlds I have 10 bits bus with a pixel clock between 10 and 60 MHz. the distance between the camera and the processor is 2 meters. That’s why I need to serialize my data
So I found the SN65LV1023A/SN65LV1224B serdes that match perfectly with needs
I still have many questions about that component:
Ideally I am looking to have an autonomous serdes system, capable to auto synchronize between them and to start crush data when they are ready. My question is about the SYNC1/SYNC2 … did they need to be driven with specific sequences? For the Deserializer do I have to look the Lock signal or it is just for information??
Do you have any application notes about? the schematics of the evaluation board? Is it possible to have the evaluation board?
What about the life time of those components??
Looking forward to have your help and your comments
Feel free to propose other references