Other Parts Discussed in Thread: TUSB2046B
hi,
i intend to use the TUSB2046BIRHB with SOM based on AM335X.
regarding pins 5,6,26.
if the data lines are disabled the component is automatic bridge for up to 4 USB ports simultaneously?
what is the exact function of pins 5,6,26 and where do i connect them to the SOM (regular I/O, I2C....)?
can u give example of using the SUSPEND pin?