This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS92LV2411 Clock source



I am using a 2412 on my product.  for testing purposes i would like to send my product non synchronous data using a 2411.  My board does not require a processor so I want to drive the clock of the 2411 with a 10MHz clock   My understanding is that this configuration should work because the 2411 is just capturing the state of the input pins ever clock period.  I can see that the 2411 is powered up, the clock is running and that the Rout+/- pins are being driven. 

 

However when I plug my device into the test apparatus, the 2412 on my device does not decode the data from the 2411.  I know that the issue is not with my device under test as the onboard 2412 functions well with it's mating product which contains a 2411.

 

My set up is as follows:

VDDIO = 3.3V; VDDTX = VDDHS = 1.8V

VDDSEL = 1; RFB = Config1 = Config2 = BISTEN = 0

De-emph = Floating

Is there anything that i am doing incorrectly?  Could the problem be with my clock source?