I am making a camera system with a processing unit and a camerahead that only contains the imager and some passives. I was looking into the DS90UB913Q/DS90UB914Q because you can put the data and communication (I2C) over 2 wires.
Is it also possible to transfer the power for the camera over the same 2 RX/TX wires between the serdes pair?
If so how can this be done? Is there some circuitry needed to connect the supply to the link?
Best regards