This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848YB Timing

Hello, could this be a data sheet typo for the falling edge of the RX_CLK in 10Mb/s Serial mode?

AC Parameter T2.14.2 RX_CLK fall to RXD_0 Delay

The minimum is -10ns and a maximum is 10ns

How can this event happen 10ns before the falling edge event?

Thanks, Gene

  • Gene,

    The timing for T2.14.2 in the datasheet is not a typo.  I will try to clarify the intent of the spec.

    Data is generated at the falling edge of the RX_CLK and should be sampled at the rising edge by the MAC.  Regarding the transition on RXD_0 / RX_DV occurring before the falling edge of RX_CLK, consider a source synchronous event inside the device.  If the RX_CLK and the RXD_0 / RX_DV edges are generated on the edge of that event, but RX_CLK has a longer output delay to the pin relative to RXD_0 / RX_DV, then RXD_0 / RX_DV will transition first when measured at the pin. 

    For an SNI MAC, the key timing will be relative to the rising edge of RX_CLK.  Another way of interpreting the timing in the datasheet is to consider the minimum setup and hold for RXD_0 / RX_DV relative to the rising edge of RX_CLK at the SNI MAC:

    • With a 35ns high time on RX_CLK and a -10ns delay relative to the falling edge, the hold time relative to the rising edge of RX_CLK will be 25ns (35ns - 10ns). 
    • With a 65ns high time on RX_CLK and a +10ns delay relative to the falling edge, the setup time relative to the rising edge of RX_CLK will be 25ns (100ns - (65ns +10ns)).

    As you can see, the timing results in relatively large setup and hold margins.

    Patrick