Other Parts Discussed in Thread: SN65HVD251, SN65HVDA541-Q1, SN65HVD255, SN65HVDA1040A-Q1, SN65HVDA542-Q1, SN65HVDA1050A-Q1, SN65HVDA540-Q1, SN65HVD257, SN65HVD256
I was looking at the
SN65HVD1050
and need to know if this supports the SAE J1939.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65HVD251, SN65HVDA541-Q1, SN65HVD255, SN65HVDA1040A-Q1, SN65HVDA542-Q1, SN65HVDA1050A-Q1, SN65HVDA540-Q1, SN65HVD257, SN65HVD256
I was looking at the
and need to know if this supports the SAE J1939.
Also note the SN65HVDA1040-Q1: http://focus.ti.com/docs/prod/folders/print/sn65hvd1040-q1.html , the SN65HVD251: http://focus.ti.com/docs/prod/folders/print/sn65hvd251.html , and the SN65HVDA541-Q1: http://www.ti.com/product/sn65hvd251 also support J1939. Just a few more choices, if you might need them.
-Leonard
Agreed. SAEJ1939 uses a High Speed CAN trasnceiver, of which all of TI CAN transciers are. As Leonard points out you can use the SN65HVDA10x0A-Q1 (latest versions in -Q1 of the 10x0 families), the SN65HVDA54x-Q1 family (541/2/3 or the -5 versions) or the SN65HVD255/6/7 if -Q1 isn't as important. I would use one of these later versions due to the updated EMC and protection features added into the designs vs previous generations, then you just need to decide on extra feature set such as CAN wake up request via RXD, I/O level shifting, silent mode, redundancy, etc.
-- Scott
SN65HVDA1040A-Q1, SN65HVDA1050A-Q1, SN65HVDA540-Q1, SN65HVDA541-Q1, SN65HVDA542-Q1
SN65HVD255, SN65HVD256, SN65HVD257