Other Parts Discussed in Thread: DP83620
We are using the seperate DP83620 to interface 2 seperate SFP modules to the iMX287
We are planning follow the below architecture for the PHY chips. Ie; using one zero delay buffer we are planning to give each of the 2 PHY chip and the iMX287 50MHz clock from a single 50MHZ sourse as in image (the image link is given below)
We are using 2 independent channels with different fiber routing.
Can anyone tell me that is there any problem in using such a configuration??
The optical transceivers we are using are operating at 155Mb/s. The processor will support maximum of 100Mb/s.
If we are following the above scheme do we have to consider additional components like FIFO between the processor and the PHY chip or not.???