Other Parts Discussed in Thread: DS15BR400
Hello !
We are developing a new projects, and we have chosen to evaluate the component DS15BR400 to drive three four channels LVDS lines.
We have valuated the DS15BR400 4-Channels LVDS Buffer. But this buffer/repeater overheat.
With a Ta = 25°C (77°F), the component reaches a temperature of 70°C (158°F) using a transfer speed of 500 Mbps and VDD = 3.3V.
Is that correct? We must expect less warm?
thanks for the support in advance,
kind regards.