Other Parts Discussed in Thread: DS34RT5110, TMDS442
I'm currently working on a design utilizing the DS34RT5110 and the TMDS442. My design involves multiple lengths of hops driven by a DS34RT5110, with each hop terminating into a TMDS442. Using the TMDS442, I break out the signal so that one signal can be used locally and then I drive another hop with another DS34RT5110. Depending on the scenario, the cable lengths between these hops can be any length, lets say from 4' up to 50'. My issue is that depending on the resolution of the signal (I am connecting these to computer outputs), the settings for the DS34RT5110 needs changed. Is there a way to "autoconfigure" the DS34RT5110, to basically detect the best possible setting for the DE and EQ lines? With the data rate depending on the resolution and the color level, I'm finding that just about each resolution leads to different settings for the DS34RT5110.