Other Parts Discussed in Thread: DP83630
Hi
What is Idd for DP83630 when pin RESET_N=0?
When will be absolute min of Idd? I don’t want disconnect Vdd…
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83630
Hi
What is Idd for DP83630 when pin RESET_N=0?
When will be absolute min of Idd? I don’t want disconnect Vdd…
We have a power measurement application note (http://www.ti.com/litv/pdf/snla089a) that details power consumption in different modes of operation. It does not include data for reset, but it does include data for power down mode. According to the power measurement application note, the device should draw approximately 7mA from the 3.3V supply in power down mode.
The device can be put into power down mode by asserting the PWRDOWN low (PWRDOWN/INTN = 0V) or by setting the the Power Down bit (bit 11) in the Basic Mode Control Register (BMCR), address 0x00. The power dissipation in power down mode should be comparable to reset, but using power down mode does have advantages when it comes to configuration:
Patrick
Patrick, thank You
In this “AN-1540” minimum current – is 7mA.
10mA (for DP83630) in Power Down – is very large for device in mobile mode when Ethernet isn’t used. Disconnect all power of DP83630 in this mode is inconveniently for me…
What will be, if I set mode “Power Down”, switch off clock (pin 34 “X1” = 0 ) and disconnect only an analog power from DP83630 (pin 19 “ANA33VDD”) and central tap of transformer?
Alexander
Alexander,
What is your target power for the DP83630 when Ethernet is not being used? Could you share some additional details on the application?
We don't have any data on the specific configuration that you suggested, but I will see what we can do. Powering down independent supply pins may not be recommended. I will inquire about this with the design team.
Patrick
Alexander,
After performing some simple lab experiments and discussing this with the design team, I believe the low current consumption achieved by asserting the power down pin and stopping the X1 reference clock is the best reasonable minimum. Powering down independent supplies is not recommended. It would be better to power down the entire chip by powering down all the supplies.
Patrick
Alexander,
In this mode, with the Power Down pin asserted and the X1 reference clock stopped, the Idd was <5mA.
Patrick